(0)| 9/5/2014 11:20 AM | |
|
Posts: 6 Rating:
|
Dear Sir Pls. Help me I wants to change the old model OP17 to New OP177B Because the old one is obsolescence The old OP17 is connected to S7300 station CPU 315 via MPI and the station also had FM357 (Position Module) to control servo drive brand Movidrive,the old op17 have the project which write by Protool software , and the New OP177B might use the winCC flexible 2008 to write, first , I open winCC flexible and open the old project file and found ,then have windows to migrate the old project file to WinCC flex file (pls see picture in attaced file) and after I click next I found the error migration E3412 (pls see picture in attaced file) The detail is in attached file pls. advise me , how to solved this problem AttachmentSimens_Support_FM357.pdf (212 Downloads) |
| 9/8/2014 11:33 AM | |
|
Posts: 4757 Rating:
|
Closed cause question posted twice. The second thread with the subject Protool migrated to WinCC Flex error E3412 (Old Protool connected to FM357)is published within the conference SIMATIC ProTool / ProTool/Pro. Best Regards Min_Moderator |
Follow us on