10/15/2014 9:01 PM | |
Joined: 5/22/2007 Last visit: 4/12/2025 Posts: 9 Rating:
|
Hi I have used a mathmatc instruction in 0BA6. In the function block there was a "reference" button so I could select a value from another block and put it in the argumentsin the mathmatic block. The program was made in Logo softcomfor V7.1 I can open the program in Logo softcomfort V8.0 and the "reference" button is still there, but when I copy the block to a new projekt the "reference" buttondisapear, and when Iselect at new block in V8.0 there is no "reference" button. so Ican only put fixed values in the arguments.How can I select a value fro another block in the arguments in 0BA8? I hope anyone can help Thanks in advance AttachmentDokument 1.pdf (277 Downloads) |
10/15/2014 9:14 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating:
|
Look here: |
Follow us on