(0)| 10/14/2014 1:10 PM | |
|
Posts: 5 Rating:
|
Hi there, Everytime, I start to run the pump, the A0501 will happen in a few seconds, then the pump stop. The attachment is the parameter setting for MM430. Any other setting that I'm missing here? Whenever the pump output is 10bar or less, the A0501 will not occured. It only happen when the pump output is more that 20bar. Hope you guys can help. Thanks.
AttachmentMM430 parameter.pdf (496 Downloads) |
Last edited by: MalaysianGuy at: 10/14/2014 1:14 PM |
|
Follow us on