(0)| 11/14/2014 4:57 AM | |
|
Joined: 11/21/2007 Last visit: 1/8/2026 Posts: 2327 Rating:
|
Hello longlan From your description and the video, it seems you are using SIMOTION D425 Motion Controller alongwith SINAMICS S120 Booksize modules . In order to connect to the System you will need the following software : SIMOTION SCOUT SOFTWARErunning on Siemens Field PG or a PC with Profibus Adaptor Cable / CP 5512 / CP 5711 etc. Additional Information : SIMOTION SIMOTION SCOUT Getting Started SIMOTION D4x5-2, Manual SIMOTION D4x5-2, Commissioning and Hardware Installation Manual SINAMICS S120 Booksize power units SINAMICS S120 Equipment Manual Booksize Power Units SINAMICS S120 Commissioning SINAMICS S120 Control Units and additional system components Hope this helps Cheers Navnag |
|
There is no such thing as the last bug in a program |
|
This contribution was helpful to
|
|
| 11/16/2014 1:45 PM | |
|
Posts: 23 Rating:
|
thank you very much
|
Follow us on