(0)| 12/4/2014 5:19 PM | |
|
Posts: 5225 Rating:
|
Hi there everyone, FOREWORD A work partner of mine identified a problem today. I wish to share it with you all. I am not actually looking for a solution.. I am hoping someone might learn for the experience. Maybe "someone" listens and identifies the reason for this occurance. BACKGROUND We are making preperations for a project that uses a LOGO OBA8 with x2 I/O extension cards. It brings the I/O count to 24 inputs and 20 outputs. My partner was preparing the LOGO program in LogoSoft V8 to contain all the loose circuits he has previously designed. The 24 inputs were already referenced, so he had to pull in the 20 outputs.. PROBLEM 19 of the outputs were pulled into the program without issue. The 20th output is giving a problem. It only states "Q" in the instruction, not the expected "Q20". We have tried varies things but can not pull in Q20 into the program. The attached file is a modified copy of this program. It would be interesting to know if others can pull in the 20 outputs into this file without the problems we had. SOLUTION (?) This problem is linked to the specific file only. My partner was able to create a clean version where pulling all 20 outputs into the program was possible. --- What are your thoughts on this? w Attachmentcorrupted file.zip (303 Downloads) |
| 12/8/2014 9:19 AM | |
|
Posts: 33 Rating:
|
Also strange is this diagram has a much smaller canvas size....how did you achieve that? Was this diagram first made in earliy versions and opened in V8? Usab |
| 12/8/2014 12:08 PM | |
|
Posts: 5225 Rating:
|
Usab, There is a thread titled: TIPS & TRICKS: LogoSoft V8 & Logo OBA8 On page 2 there is a title: [LINK] (Date Code: 11/20/2014, 10:38 PM) WORKING WITH MULTIPLE PAGES IN A PROJECT That will answer your question. Spoiler: It is a printer setting. Greetings. w |
| 12/8/2014 1:44 PM | |
|
Posts: 33 Rating:
|
I see, I am not even aware of this possibility. Usab |
This contribution was helpful to
|
|
Follow us on