(0)| 12/28/2014 11:02 AM | |
|
Posts: 2 Rating:
|
In order to start up the control system of a distributed generation gas power plant, I have a common PLC which is in relation with 3 specific PLCs for control of 3 engines. ( diagram is attached) All CPUs are 316-2DP. The memory card of common PLC is 6ES951-1KH00-0AA0 But unfortunately memory card of those 3 PLCs are lost and i should prepare memory card for them. But unfortunately this memory card is obsolete and i couldn't find one. I was wondering if it is possible to replace this memory card with a memory card with this code : 6ES951-0KJ00-0AA0 This one is available and I can prepare it easily. So is it possible to prepare 0KJ00 memory for those 3 PLCs ??? and won't be there any problem in compatibility ?? many thanks for your time and concern Attachment1-3.pdf (263 Downloads) |
| 12/28/2014 3:47 PM | |||||||
|
Joined: 9/27/2006 Last visit: 1/15/2026 Posts: 12481 Rating:
|
Hello Milad; Your CPUs must be very old, at this time all MCs 951 seem to be in discontinuation phase, and if they csn be found in Siemens' distribution centers they will be very expensive.
SIMATIC S7, MEMORY CARD FOR S7-300, SHORT VERSION, 5V FLASH EPROM, 512 KBYTES Which memory cards can you use with an S7-300 CPU? You could try to find these EPROM modules on the web, there are many resellers of automation equipment that hold these items. For example: https://www.google.ca/#q=6es7951-0kj00-0aa0^ Hope this helps, Daniel Chartier |
||||||
| 12/28/2014 5:52 PM | |
|
Posts: 784 Rating:
|
Hello, Perhaps thislinkmight help. CPU 316-2DP Order no. 6ES7316-2AG00-0AB0 Type of memory card MC max. 4MB 6ES7951-1KH00-0AA0 SIMATIC S7, MEMORY CARD FOR S7-300, SHORT VERSION, 5V FLASH EPROM, 256 KBYTES 6ES7951-0KJ00-0AA0 SIMATIC S7, MEMORY CARD FOR S7-300, SHORT VERSION, 5V FLASH EPROM, 512 KBYTES So,the 2 types of MC can be used withCPU 316-2DP Best regards |
| 12/29/2014 5:49 AM | |
|
Posts: 2 Rating:
|
noted and Thanks :-) kind regards Milad |
Follow us on