1/6/2015 8:32 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of the User DShailendra
|
1/6/2015 9:31 AM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16461 Rating:
|
Hello You neet at least WinCC flexible 2008 to program this device. look at this technical information: http://support.automation.siemens.com/WW/view/de/30699225/td/en Here you can find at the caption "Configuration software" which software you neet to program the panel. There are no device files which you can import to your older WinCC flexible Version When you need also help to transfer the project to the Panel you can use this FAQs: http://support.automation.siemens.com/WW/view/en/23802405 http://support.automation.siemens.com/WW/view/en/23800567
regards Murof ------------- When this information helps, you could use the Rate Button |
Last edited by: Murof at: 1/6/2015 9:32 AMIf this Information really helps, you could use the Rate function |
|
Follow us on