(0)| 1/7/2015 7:42 AM | |
|
Posts: 179 Rating:
|
dear experts please help me to solve this issue 1-i have a bcu 6md64 connected in substation using SAS SICAM PAS,and wincc. unfortunately one of the binary input of this BCU which connected to the CPU card not working but in general the bcu working well communication and every thing connected to scada OK ,so i tried to order a new card ,then i replaced the card ,initialize my digsi project ,and every thing seems OK normal led .no error . the problem is that i have allready a cfc to get the status of the BCU , see attached file,but unfortunately this output not executed it seems something inside the BCU not working probably . i also notice that something wrong see attached snapshot file showing the behaviour of the BCU. GW IP 172.16.0.254 and my NT1 is 172.16.0.21 it appears on all BCU on the substation like this but for this BCU strange value appear , you will see GW and NT1 are the same i don't why and also corrupted parameter appear some and disappear ?????i download this file digsi to another BCU and it is working fine IP OK status OK ,CFC OK thanks to provide me a solution Attachmentsnapshoot.zip (521 Downloads) |
Follow us on