1/8/2015 8:32 AM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16436 Rating:
|
Hello adhey dogra This problem sounds strange. Usually the User Management will be importet when you start the Runtime. So you cant try to transfer the project and overwrite the User Management. you could also generate a new *.pwx file in the WinCC flexible project and than overwrite only the pwx Data (you have to rename the File in PDATA.pwx). But when you don´t have the project or WinCC flexible Engineering I don´t know what to do.. ---- At your Problem with the Licence Manager you could try to deinstall it an install the current Version on this Support Pages: http://support.automation.siemens.com/WW/view/en/114358 I hope it helps a little bit Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on