(1)| 12/2/2014 11:13 AM | |
|
Posts: 4 Rating:
|
Hello experts, I am quite the novice I have to admit, so excuse my question if it is a stupid one; Is there any way to change or disable or hide the cursor for a KTP700 in TIAportal? it has WINcc basic. I can find non of the above stated options and I have used the search function in the PDF manual to no avail. Thanks in advance for you help.
----------- new subject after splitting from Changing the MOUSE pointer in WInCC |
Last edited by: CS Moderator at: 12/3/2014 10:14 AMsplitting |
|
| 12/3/2014 11:58 AM | |
|
Posts: 5225 Rating:
|
Hi there. Recently we were doing a project with the KTP700 Basic Panel. We were looking for the same type functionality. It seems as though this "2nd generation" HMI does not have teh ability to hide the mouse cursor. I am however very sure I saw the setting in the Windows CE options of a older HMI (KTP600?). It is however fair to mention the "2nd generation" HMIs do not run on Windows CE. ..so it is a case of grin and bear it. w |
| 12/22/2014 11:57 AM | |
|
Posts: 4757 Rating:
|
|
Follow us on