11/10/2014 8:42 AM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello Q-think, we would recommend to create a Support Request at the customer support. They will know, which parts need to be used for the upgrade. |
With best regards, |
|
11/20/2014 12:46 PM | |
Posts: 1 Rating:
|
Hello Q-think, would you like to share the solution with us? Did youhave to change the power block? Thanks |
1/15/2015 10:15 AM | |
Joined: 3/11/2014 Last visit: 1/27/2025 Posts: 1 Rating:
|
Hello! To upgrade the CIB to CIM you should NOT change the CU320. If your converter is 500-690VAC you may need to upgrade the FW to >V2.6.xHF11 because of problems handling DC-link ripple in older versions. See this link to find the CIM and appropriate IPD-card. CIM is always the same, but IPD defines the converter type. http://support.automation.siemens.com/WW/view/en/35495618 |
Follow us on