(0)| 5/16/2012 2:20 AM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Marif; In answer to your question about redundant IM 153-2: See the following FAQ, especially the section on redundant DP/PA link hardware: How is the DP/PA link structured? To have redundancy in any arrangment of 2x IM 153-2 (Y-Link, DP/PA link) you need to have an active backplane bus for the IM 153-2s and the required coupler.Study theFAQ above, and check if you have the required active bus modules and the special support rack for them in your project. Hope this helps, Daniel Chartier |
| 5/16/2012 4:00 PM | |
|
Posts: 4 Rating:
|
The address on both SMAR seems OK and matches the address on Hw Config (7 and 8) which can be seen after the power on. |
| 1/20/2015 11:37 AM | |
|
Posts: 4757 Rating:
|
|
Follow us on