(0)| 1/20/2015 2:20 PM | |
|
Joined: 10/11/2006 Last visit: 1/16/2026 Posts: 6068 Rating:
|
Hello, Fast I/O on Simotion Integrated or CU320-2 has the same repeatability ( ca. 5us). It doesn't 't depend on the cycle time. The cycletime of the D425-2 with 1 Virtual Axis, 1External encoder and 2 Camming axis is 1ms; If you program SCL, you will have less problem with the ST-Code of Simotion, because it is similary. There is an example application available. http://support.automation.siemens.com/WW/view/en/37706606 Your local siemens guy can provide youwith the software. https://www.automation.siemens.com/aspa_app/?ci=yes&HTTPS=REDIR®id=WW&lang=en&comptcid=o When you want to use PLC, it is necessary todo the fast parts on drive side (DCC). Without an example, I wouldn'ttry this, because I doesn't know whether all is possible. |
|
With best regards, |
|
This contribution was helpful to
|
|
Follow us on