(0)| 1/27/2015 5:09 PM | |
|
Joined: 7/7/2010 Last visit: 1/16/2026 Posts: 16379 Rating:
|
At this point, send your project to Siemens via Support Requestso they can evaluate and see whether V13 SP1 will compile your project without crashing. If so, they fixed the problem with SP1 and will recommend you upgrade. If SP1 fails to compile, they can then fix the problem for everyone. In the meantime, your resistance to rebuild (in the same project) the PLC hardware, settings, and configuration, then copy over all the OBs/FBs/FCs/DB/tags/watch tables, etc. to that new plc is only going to slow down progress. I have a very recentproject that required doing that very thing. In under an hour I was able to migrate everything, compile, download, start, and get moving forward. Yes, it was a wasted hour, but if I did not do that, I would probably still be waiting for a solution that made sense to me and my customers. Please post progress as you make it. |
|
science guy |
|
Follow us on