(0)| 2/11/2015 8:59 AM | |
|
Joined: 2/10/2015 Last visit: 10/17/2025 Posts: 3 Rating:
|
Hi Mehadji, the channel 4 of the module with base adress 368 has been passivated. But the last error is outgoing event (The error is gone, and the module is no longer passivated) The reason for passivation depends on your configuration and when the error has not yet been acknowledged you can check it by going online on the module in hardware config. Either it's a channel evaluation error (1oo1, 1oo2 evaluation), discrepancy error, programming error, short circuit, overload, wire break etc. After a channel has been depassivated the channel needs an acknowledge (via FB219 for example) if you have configured this in HW config for the channel. Check this manual for further info. https://support.industry.siemens.com/cs/#mdm/22099875?c=56880428555&lc=en-US |
Follow us on