(3)| 2/12/2015 4:28 PM | |
|
Posts: 47 Rating:
|
@huggy_d1: Thank you for your answer. The fact is that I'm porting to TIA portal a project realized on Step7 v5.5, therefore I was trying to follow the same hardware configuration. In that project the IM 151-3 PN is connected to the CPU via profinet, and the the addresses of the input modules are consecutive. So there should be a way to accomplish this without moving the input nibbles in a single word as you suggest.
Anyway thank you again ChristophD! |
Last edited by: dan90 at: 2/12/2015 4:33:46 PM |
|
This contribution was helpful to
|
|
Follow us on