(0)| 3/2/2015 3:09 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello Alireza; This is how this encoder is described in Siemens Product support (look it up yourself if you want more détails, manuals or FAQs, simply do a seach with the part number iin the Search box at the top right of this page): 6FX2001-5QS12 ABS ROTARY ENCODER 6FX2001-5QS12 SSI ABSOLUTE VALUE ENCODER SINGLETURN 13 BIT WITH SSI, OPERAT. VOLT. 10-30 V STRIP FLANGE SHAFT 10MM RADIAL FLANGE SOCKET Basically, this encoder model does not come with a Profibus-DP interface. You need an SSI interface in your Simotion controller to connect it, with RS-422 standard connectivity. This link will show you general information ion SSI encoders: Synchronous Serial Interface - Wikipedia
If you have any doubts about Siemens absolute encoders with and without SSI, this comparative datasheet should be of help: http://siemenssale.com/content/?297.html
Notice that absolute encoders with part numbers buiolt on the structure "6FX2001‑5.P.." can be connected to profibus-DP, as you already showed in your original question. Hope this helps, Daniel Chartier |
Follow us on