(0)| 3/23/2015 2:24 PM | |
|
Joined: 11/29/2011 Last visit: 2/4/2025 Posts: 1362 Rating:
|
Hi, Extract from the manual SIMATIC HMI HMI device MP 277 chapter "7.6 Backup and restore" : "Backing up and restoring by means of external storage device The "Backup / Restore" function is approved for MMC and SD memory cards as well as USB mass storage devices. " Also have a look at Which external storage media can you use with the current SIMATIC panels and which memory card interfaces do they have? link to see what options you have. I hope I could help a bit. |
|
- What you read here, please check with manuals and your requirements. |
|
Follow us on