(0)| 4/20/2015 9:30 PM | |
|
Posts: 1 Rating:
|
Can anyone help? I have a very basic operating manual that was translated to English but it has been little help. I have made some very basic wiring diagrams for my own use but I’m not sure what help they will be to you. This machine came from China a while back and no further information was given so it may be difficult to explain. We have not yet used the machine because we just finished re-building it from the ground up. All components get power and work correctly but we are unable to get beyond cycling them on for testing due to the language barrier. As stated earlier I think that we are only seeing tier 1 of 4 and that our access to areas where the process is refined is not being authorized. As far as I know the S7-200CN worked effectively and we do not need to upgrade unless that is our only option. Ideally I would like to just change the language and gain access to all levels if possible? If this is not possible what options do we have to get this machine up and running as quickly as possible? Is the US version of the Micro/Win software able to convert our process?
---------------------------------------------------------------------------------------------------- |
Last edited by: RTM001adam at: 4/20/2015 9:39:58 PMLast edited by: Min_Moderator at: 4/21/2015 3:20:22 PMNew subject after splitting |
|
Follow us on