(1)| 5/4/2015 4:30 AM | |
|
Joined: 6/8/2011 Last visit: 12/2/2025 Posts: 2 Rating:
|
Step 7 Microwin SP9 can support windows 8.1 yes or not ? |
| 5/4/2015 6:30 AM | |
|
Posts: 4620 Rating:
|
Hello Dragonfly, Please have a look: Which+version+of+STEP+7+is+compatible+with+which+ ... - Siemens |
| 5/4/2015 7:17 AM | |
|
Posts: 5225 Rating:
|
Ste39 - You are making a VERY good suggestion there. Personally I downgraded from Windows 8 to Windows 7 on my PC AttachmentSTEP-7-Micro-WIN_V4.0_compatibility-list_en_2015-04-27.zip (504 Downloads) |
Last edited by: William_B at: 5/4/2015 7:17:46 AMformat |
|
This contribution was helpful to
|
|
| 5/4/2015 7:38 AM | |
|
Posts: 4620 Rating:
|
Hello William, Thanks for your comment, I found this on another forum, I translated into English, if can help to someone ... MICROWIN SP9 and WINDOWS 8.1 Translation: I tried just now and it works; unfortunately indicates that mistake for communication, Windows 8.1 with the .bat launched an error that can not access the device; but I have a stubborn, so I wanted to try to run the command by hand; I tried to do the file in question (s7epaImp64x.exe) and I ran the command as it was reported in the bat file and now works with the USB Serial cable (with USB / serial adapter - my PC does not have the serial port) ; the command at least for this PC I have, is: quote: C: \ Program Files \ Common Files \ Siemens \ Automation \ Simatic OAM \ bin \ s7epaImp64x.exe Finally, I want to remember that when I installed MicroWin, with the only version 4 did not succeed: I served MicroWin 4 SP9. |
This contribution was helpful to
|
|
Follow us on