5/15/2015 2:28 PM | |
Joined: 1/15/2014 Last visit: 8/26/2025 Posts: 1 Rating:
|
Hi, I don't have a solution I'm afraid but I do have the same problem on 6 plc's. The last machines I used this program on were pre SP1 update and were OK but since SP1 I have this fault. Any help would be much appreciated. Screen shot added. Cheers Ade |
5/15/2015 4:00 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, normaly this message means that a IO-Device is returned to the BUS and have a peripherial error on a submodul. In the Screenshot in the second post you see the HW ID which set the diagnostic, so look in your project which device is connected to the Port2 of you X1 Interface and have the HW ID 66. This device you must diagnostic.
|
5/15/2015 4:20 PM | |
Joined: 7/7/2010 Last visit: 9/12/2025 Posts: 16094 Rating:
|
My most common problem during upgrading like you are doing is profinet configuration defaults to some unacceptable IO update time. Raise that value until the plc compiles, downloads, and runs properly. I think this is fixed in V13 SP1 with the latest updates.
|
science guy |
|
Follow us on