(0)| 5/26/2015 9:39 AM | |
|
Joined: 1/4/2007 Last visit: 1/13/2026 Posts: 1198 Rating:
|
Hello Rajnish,
Please use the Siwarex FTA in place of Siwarex M.
Unfortunately you have to change your PLC program, because the Siwarex FTA has another DB_Scale, other command codes, … .
The block “Siwa-FTA” is protected! You can’t open this block. This block is handling the communication between the PLC and the Siwarex FTA module. But it is not necessary to open this block, because you need nothing to change regarding the communication.
I recommend you to use the Siwarex FTA example project on the internet: https://support.industry.siemens.com/cs/ww/en/view/25296061
You can use the following addresses into the DB12 (=DB_Scale) to execute a command: - to set the command code: DB12.DBW40 - to execute the command: DB12.DBX42.0
Which kind of problems do you have exactly on the scale?
Best regards
Siwarexi |
Follow us on