(0)| 5/26/2015 10:57 AM | |
|
Posts: 3 Rating:
|
Hello, I have update Step 7 V5.5 to SP4 in order to open a PLC program developed with this version. That is ok for this one in order to see the program online on TCP/IP protocole PG/PC. But now, a new problem arrived, I can not communicate on PC Adapter MPI yet (before SP4 update, MPI communication was running). I tried to re-install PC adapter USB software, but I meat the error : "The wizard was interrupted before PC Adapter USB could be completely installed." Do I need something on more in order to install adapter USB on Windows 7 Professionnel SP1 ? In PC adapter USB readme, I don't see Win 7 like compatible OS . Is there an update for Win 7 ? What could you suggest to solve my problem ? Thanks per advance. Nadege
---------------------------------------------------------------------------------------------------- |
Last edited by: U_7d08dc48-03b1-4fb2-9e7f-0394fae9415e at: 5/26/2015 10:58:29 AMLast edited by: Min_Moderator at: 5/27/2015 1:15:42 PMNew subject after splitting |
|
| 6/2/2015 9:42 AM | |
|
Posts: 3 Rating:
|
Thanks to create for me a new post. I still have the same problem, can you help me for that ? Nadège |
Follow us on