(0)| 6/8/2015 10:48 AM | |
|
Posts: 4 Rating:
|
Hello freinds I have a big problem I installed BData application server on a separate PC and the BData acquisition on an other PC , I added a hardware acquisition in the first PC( Name of the host is the name of the PC on witch I installed the application server) In the wizad interface , I chose Modbus and I selected "used defined configuration" , The IP port was by default 502, ( I have known that BData componements connect via 4444 port !!) I entered the IP adress of the second PC and the device name (PC with acquisition componement) but an error message appears "unreacheable device" alhough The acquisition PC appears in the network and I can ping to its IP adress . Is my configuraion correct ? what shall I do , please help me Thanks ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/8/2015 4:14:31 PMNew subject after splitting |
|
Follow us on