(0)| 6/22/2015 4:01 PM | |
|
Joined: 8/3/2009 Last visit: 1/20/2026 Posts: 16644 Rating:
|
Hello DavidBrown You cannot get a direct access to the filesystem of a Simatic Panel. The only Posibillity is to use the Miniwebsites of the Panel (activate Option Webpages; has nothing to to with Sm@rtServer). With a login in the Webpage o nthe Panel you can click toa file system browser an get a manual access to the files on the Panel or the External storage devices. You need to run the Websites a Sm@r Service License but for testing it works without license The other Way ist to get Access from the Panel to a storege Device of another PC in the Network Look at this FAQ: https://support.industry.siemens.com/cs/ww/en/view/92346478 Wish a nice day Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on