(0)| 5/20/2010 3:32 PM | |
|
Posts: 29 Rating:
|
hello. I've encoutered the following problem. I didn't used S7-200 till now, andI have to implement a motor direct online function. The problem is that ifI use the subroutine only one time everything goes perfectly, but when I use it again the problem appers. What is the problem.....I think I know, but I don't know how to solve it. The problem is: the subroutine uses local variable for input and output: l0.0=> l1.5- 10 inputs, 4 outputs. When I start one motor, the outputs of all subroutines(I use it 8 times) are in high state. I read here on forum that this problem apears from set instrunction. I modify the function,but the problem persist. I attach the subroutine.Hope that you can help me. Thank you Attachmentsubroutine.zip (830 Downloads) |
Last edited by: meTRAIAN at: 5/21/2010 8:53 AM |
|
| 5/21/2010 8:58 AM | |
|
Posts: 29 Rating:
|
The seconds subroutines is the same as first, only formally parameters(inputs and outpus) are different. |
| 5/21/2010 1:23 PM | |
|
Posts: 29 Rating:
|
i attach the project. for testing i introduce 2 more subroutines, to test some simple networks.
AttachmentProject1.zip (614 Downloads) |
Follow us on