(0)| 9/4/2015 2:52 PM | |
|
Joined: 3/2/2007 Last visit: 1/20/2026 Posts: 1004 Rating:
|
can we run a 1PL6 motor with a G120 sinamics drive ? any problem will happen ? SIMOTICS M COMPACT INDUCTION MOTOR; IP 23 OPERATION ON MASTERDRIVES VC/MC CONVERTER WITH EXTERNAL FAN HTL INCREMENTAL ENCODER 1024 P/REV 89 KW, 1750 RPM, 486 NM (VC) TERMINAL BOX ON TOP CABLE OUTLET ON THE RIGHT SIDE DESIGN IM B 35 W/O BRAKE DEEP-GR. BALL B.,VIBRAT. SEV. R SHAFT/FLANGE ACCURACY N FEATHERKEY A. SEMI-WEDGE BALAN. AIR FLOW FROM D-END TO ND-END STANDARD PAINT FINISH: RAL 7016 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/4/2015 3:27:54 PMNew subject after splitting ... thank you ... |
|
Follow us on