(0)| 1/23/2008 7:09 AM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello Floyd: I am far from being an IT expert, so all I can do is point you to the following manual: CP 243-1 IT Communications Processor for Industrial Ethernet and Information Technology It discusses changoing the operating parameters of the CP 243 through the user program, but gives these 2 important caveats: -any change to the parameters through the user program will become effective only after CP reboot; -changing the IP address (amongst other things) trhough the user program involves disabling the CRC logic of the program, so there will be no garanties that the module works properly afterwards. In any case, it should give you enough to start asking more precise questions for your application. Hope this helps, Daniel Chartier |
Follow us on