(0)| 10/4/2015 3:41 PM | |
|
Posts: 9 Rating:
|
hello we use g150 j type drive(parallel operation converters),2 winding motor,2 separate line module(AC/DC),two separate MM(DC/AC). while starting the drive unit immediately drive triggering the fault f30002 (Vdc over voltage fault).i done capacitor reforming also.then also i am getting same fault in one motor module only plz find i am attaching drive backup.inform me any parameters want to change Attachment420fn01_29_9_2014.zip (228 Downloads) |
| 10/6/2015 1:41 PM | |
|
Posts: 4757 Rating:
|
Closed cause question posted twice. The second thread with the subject G150, Fault f30002 is published within the conference SINAMICS. Best regards Min_Moderator |
Follow us on