(1)| 6/24/2010 9:23 AM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello erkanozdemir, You have to install the driver of the PC adapter. It normally came with a CD that contains the driver and also here's a link for it. Driver and Firmware for PC Adapter USB 1.2 Hope this helps. |
|
Ayman Elotaify |
|
| 6/24/2010 9:30 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
You didn't mention what are settings which you already did. What is the error when you try to connect... I suggest you to start with Working with STEP 7 V5.4 Getting Started. Also you could use "inbuild" manuals in Step7 installation directory (bassically this is C:\Program Files\Siemens\Documentation\English) Best regards, Hristo Mihalev |
| 6/24/2010 2:20 PM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hello, You should install Authorization on harddisk. Perhaps this link might help: how do you install, uninstall and upgrade authorizations? Best regards, Wizard |
| 6/25/2010 10:52 AM | |
|
Posts: 19 Rating:
|
i couldn't reach to floopy disk so if it is possbile could you send me it with mail or here have a nice days |
| 10/22/2015 2:18 PM | |
|
Posts: 4757 Rating:
|
New question published by nppesn is split to a separate thread with the subject Compatibility USB/MPI+ V4.0 and windows 7 x64. Best regards |
Follow us on