(0)| 10/31/2015 9:00 PM | |
|
Posts: 1 Rating:
|
Hi guys I'm having some troubles with my TIA v13 and the TP. I keep getting the same error, every time I try to download to the TP900. The setup is a 1500PLC to a TP900 over profinet. I can compile, when I'm not referring to the PLC from the screen, but, if I make a pushbutton or similar, it comes with the error. The PLC makes a "loose end error", cause it can't see the neighbour I've attatched some pics of the errors Thanks a lot AttachmentCompiling error.zip (135 Downloads) |
Follow us on