(0)| 2/5/2008 12:01 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
hello augel Sorry, to my knowledge you cannot use the Prosave file on anything other than another OP27. One option, if you are satisfied with the application as it is running on the old OP27, would be to replace the back-light CCFL tube in the OP27. The attached drawing has info on that. You could also look for a refurbished OP27 on the market, and download the Prosave file to that unit. There are many vendors on the web, for example look at the selection here (I have never worked with them, as I did mostly business in North America): http://shop.softwerk.at/product,75,OP27.html If you need to modify the application, then you need to think new panel, and probably new software, certainly some hours to rebuild the application from scratch. Hope this helps, Daniel Chartier |
| 2/7/2008 8:15 AM | |
|
Joined: 1/25/2007 Last visit: 1/14/2026 Posts: 6 Rating:
|
Hello, thaks very much, I have requested supply of moduldisplay. Somebody knows how make it???? (see attachment) Best regards AttachmentOP27 turbina.zip (746 Downloads) |
Follow us on