(1)| 9/3/2009 2:47 PM | |
|
Joined: 6/8/2007 Last visit: 12/30/2025 Posts: 41 Rating:
|
I have to Prosave an old TP170A(V5.2.0.24) Panel and restore the file to a new spare part(V7.x) of TP170A I try to prosave it but failed when i using the Prsave V7.4.4. Then i found a document indicated the problem should be the image version with wrong prosave version which means i need to install the protool version V5.2 SP1 and do again maybe.. But i don't have such old prosave tool... and even though i have it and backup successfully. Is that possible to restore the file into new spare part ?? What should i do ? AttachmentProTool_Image_Versions_e.pdf (443 Downloads) |
| 11/29/2015 8:08 PM | |
|
Joined: 3/28/2015 Last visit: 1/4/2026 Posts: 727 Rating:
|
Hello, Resetting the Operating System to the Factory Settings. I advise you to do it using ProSave V13 Perhaps the following topics might help: 1-How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels?2-Servicetool SIMATIC ProSave |
|
Eng.Mohamed Ibrahim |
|
Follow us on