(0)| 12/8/2015 1:43 PM | |
|
Joined: 6/22/2009 Last visit: 6/6/2025 Posts: 63 Rating:
|
Hello, I want to connect WinCC OPC Clients to OPC Server over internet. The OPC server will be Telecontrol Server Basic (8 clients). This is required as the customer wants access to visualization and control of the S7 1200 stations from different locations. The configuration I have thought is attached. I think only RT128 Wincc Adv V13 will do on the remote OPC Clients. Will this configuration work? Or is there a better configuration? Regards AttachmentTelecontrol.pdf (250 Downloads) |
| 12/9/2015 7:25 AM | |
|
Joined: 6/22/2009 Last visit: 6/6/2025 Posts: 63 Rating:
|
Thanks. Alternatively, I can have a Sm@rtServer License on the Central PC. And I can run upto 5 Sm@rtClients on PC based WinCC RT Adv over internet. Will this work? Regards AttachmentTelecontrol1.pdf (249 Downloads) |
Last edited by: bits_n_bytes at: 12/9/2015 7:40:25 AM |
|
Follow us on