(0)| 12/15/2015 2:37 AM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Grzegorz; If it is only the Profibus communication aspect of the migration that bothers you, there are a few differences between the MM440 interface and the G150, but the structure is similar. See thhe following discussion for a basic view of the situation, and check out the mpre complete information presented in the G150 operating manual ( and the S120 Function manual attached below): https://support.industry.siemens.com/tf/ww/en/posts/23103/
SINAMICS G150, Converter Cabinet Units 75 kW to 1500 kW, Control version V4.7 https://support.industry.siemens.com/cs/ww/en/view/104961375 Sinamics S120 Functions manual: |
This contribution was helpful to
|
|
Follow us on