2/15/2008 12:26 AM | |
Posts: 46 Rating:
|
Hi all, I am using WinCC to connect to S7-200 via IE/OPC. Well I'm not on to the WinCC part yet, still stuck on the bleedin' OPC I have already read several dozens of FAQs and forum threads, not to mention that I followed all the step by step guides and app. notes while commissioning the setup. All with limited success. I can ping the CP243-1 from the PC station and also connect to the CPU224 via IE using Step7 Micro/Win. Since I cannot get the OPC Scout to work on the damn thing, I must be doing the config at one or both ends wrong. How can I do further fault finding??? The PC station (WinCC V6.0 + SP3 + HF2) is runningon Win XP +SP2 with Step7 V5.3 + SP2 and Step7 Micro/Win V4. I would appreciate any help you can offer on this problem. I included some screenshots, configs etc. in the attachement - hope it helps. Best regards, Ragud AttachmentS7-200_OPC.zip (604 Downloads) |
Follow us on