(0)| 1/3/2016 1:03 PM | |
|
Joined: 12/22/2012 Last visit: 10/13/2025 Posts: 92 Rating:
|
Hii all, I have a project with 1212c v4.1+ 3 g120 drives equiped with Cu250SPN V4.7.3. I wanted to communicate with 3 drives same as demo which is "70155469_SINAMICS_G120_CU250S2". I wanted to create new configuration contains one cpu and one drive (just one for starting step now) as same as demo project but it is impossible. Why? Let me explain with another way. Its is impossible to create a new project as same as 70155469 application. Why? But I can not modify process image as "Cyclic PI" as demo system. Because not have at my options as you see at the attachment. Also systems constant parameters are not same. You can see demo and my config at the same page. Another most important issue is why raad/wrt addresses are so far away from profinet address I256, Q256. But communication FC has an address 275 which is far away from I256 and Q256. All are confused me. Because when I add 2 drives more, All read write addresses are conflict each other. My portal is V13+SP1+UD6. Do you have some detailed documentations to advise. Have a happy new year to all of you.
Attachmentg120-1200.pdf (217 Downloads) |
Last edited by: corkscrew2 at: 1/3/2016 8:27:30 PM |
|
| 1/5/2016 6:46 AM | |
|
Joined: 5/12/2006 Last visit: 1/21/2026 Posts: 22829 Rating:
|
Hello, for direct HMI Access to Sinamics drive please refer this FAQ: https://support.industry.siemens.com/cs/ww/en/view/29522676 HW-ID: loop control: have you downloaded the configuration to the drive without error? Regards Christoph |
Follow us on