(0)| 2/11/2008 4:45 PM | |
|
Posts: 6 Rating:
|
Hi everyone, I've a problem with NCM PC Wizard... I'm trying to make my network architecture with NCM PC Wiazrd. I've a CP1616 and a CU320, a smart line module and a double motor module (6SL3130-6AE15-0AB0) with two motors+sensors (6SL3120-2TE13-0AB0). All is linked with DRIVE-CLiQ. In a new project I added the CP1616 in the rack, then I inserted a PNIO system. And now I don't know what to do !! The first problem I met was to find the gsd files related to my stuffs. I imported them from the Compact Flash card and I installed them, but I can't add the CU320... Actually, the file is "gsdml-v2.1-siemens-sinamics-s-cu3x0-20070726.xml" but like it's a 2.1 version, a window tells me that the date will be set to the 2.0 version in order to be readable by the software version I had (NCM-PC 5.4) [by the way, this windows appears in German in spite of the language set to English ;-)] So, I tried to install a CU310 instead of the CU320...and it was possible ! The GSD file for the CU310 is a v2.0... and I could add the CU310 in my architecture, only after having created a subnet. So, the questions are : _ Why did I have to create a subnet ? I'm using a CP1616 with 4 ports... _ How to install the gsd for the CU320 ? _ And what's next to do after ? Can I load this configuration right after that ? obs : I attached two screenshots, one of the architecture in NCM, and another of the architecture in NetPro. Best regards, TB. AttachmentNCM.zip (553 Downloads) |
Follow us on