1/15/2016 1:07 PM | |
Posts: 18 Rating:
|
Hi, As per your guidelines i have checked parameters, p1300 is 21 and encoder ppr is 1024 which is matching with the installed one. but there is some difference between r60 and r61 when it is running. For your reference i have uploaded the following for your reference. can you please advise where we are doing the mistake. 1. Starter application back up of the motor. 2. Encoder nameplate details 3. Starter Screenshot of motor encoder and expert list. regards, KK Attachment12dr1__1.zip (177 Downloads) |
This contribution was helpful to
1 thankful Users |
1/15/2016 1:16 PM | |
Posts: 18 Rating:
|
Screenshots & Encoder info
Attachmentattach.rar (177 Downloads) |
1/20/2016 12:25 AM | |
Posts: 18 Rating:
|
Please offer assistance on this subject. |
Follow us on