2/6/2016 8:07 PM | |
Joined: 9/27/2006 Last visit: 9/21/2025 Posts: 12420 Rating:
|
Hello Saeed; Have a look at the following Application Example, it might provide a good deal of hints for your project: SINAMICS G: Positioning a G120 CU250S-2 with S7-300/400 (STEP 7 V5) via PROFINET/PROFIBUS using Safety Integrated (via PROFIsafe) and HMI https://support.industry.siemens.com/cs/ww/en/view/68109071 Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
2/7/2016 12:57 AM | |
Joined: 9/27/2006 Last visit: 9/21/2025 Posts: 12420 Rating:
|
Hello Saeed; The application I sent you uses FB283 for acyclic communications between the S7 CPU and the G120 , and is used for EPOS control.I am not sure how you can use only cyclic communications for EPOS control. But if you want to try only cyclic (Profidrive) comms, see how they are defined in the following manual (there is a section on Profidrive exchanges), and decide if you can achieve your goal this way. Function Manual Basic Positioner https://support.industry.siemens.com/cs/ww/en/view/109477922 Hope this helps, Daniel Chartier |
Follow us on