(0)| 2/8/2016 2:53 PM | |
|
Posts: 31 Rating:
|
Hello Christoph, I would like to run the torque control. in the attachment you can find the pictures related to the connections and also program starter. according to sinamc picture, I get the connection between X132 with 24V and also X133 with 24V. but according to the picture"control logic" I chose r722.0. from inputs/outputs for the X132 i chose r899 bit 12. when I connect the blue wire(from X132) to 24V, the terminal evaluation works and the loght is tun on but for X133 by connecting the Black wire to 24V the light for DI 0 does not turn on and it seams there is no connection with program by X133. Thanks in advance for your help AttachmentNew folder.zip (199 Downloads) |
Follow us on