(0)| 2/4/2016 12:13 PM | |
|
Posts: 147 Rating:
|
Thank you so much. I believe I can use one of the cards for the central cpu rack ? like this one below http://w3.siemens.com/mcms/sensor-systems/en/weighing-systems/weighing-electronics/plc-based-weighing-modules/Pages/weighing-module-siwarex-wp231.aspx Does this WP321 support my load cell? and how can I tell if WP321 is for ET200SP or ET200S ? is there any thing that I can distinguish it by? SIWAREX WP321 WEIGHING ELECTRONIC (1 CHANNEL) FOR STRAIN GAUGE LOAD CELLS / FULL BRIDGES (1-4 MV/V) FOR SIMATIC ET200SP, FITS TO BU-TYPE A0, RS485- INTERFACE FOR CONNECTION OF SIWATOOL OR A REMOTE DISPLAY
|
Last edited by: AUTOMOTO21 at: 2/4/2016 12:15:01 PMLast edited by: AUTOMOTO21 at: 2/4/2016 2:35:15 PM |
|
| 2/4/2016 2:45 PM | ||
|
Joined: 10/4/2007 Last visit: 9/9/2025 Posts: 18 Rating:
|
Hi The WP231 can be used as "Stand alone" weight, where you communicate via ModBus TCP or you can use togehter with S7-1200 ET200SP
|
|
| 2/5/2016 11:17 AM | |
|
Posts: 147 Rating:
|
hahaha I have a problem reading descriptions that are not in points but instead a full connected text 😂. thank you so much |
| 2/17/2016 12:10 PM | |
|
Joined: 1/4/2007 Last visit: 1/13/2026 Posts: 1198 Rating:
|
Hello AUTOMOTO21,
Currently, there exist no Siwarex module for ET200MP.
But there are some Siwarex modules available for S7-1200 PLC: 1. These Siwarex modules can be connected beside the S7-1200 PLC. - For static weighing: Siwarex WP231 module. - For a belt scale application: Siwarex WP241 module. - For a dosing application: Siwarex WP251 module.
2. Also you can use the WP321 module for static weighing in ET200SP with a S7-1200 PLC.
Best regards
Siwarexi |
Follow us on