(1)| 3/11/2016 11:36 AM | |
|
Joined: 5/31/2011 Last visit: 8/7/2025 Posts: 190 Rating:
|
Got a workaround: NirCmd Freeware utility (download at the bottom). Create a ".bat" file "CloseExplorers.bat" with the following command:
Then in TIA a script where you call up the .bat file:
You can then execute the TIA script at the "press" event off a button, or through the schedular at a screen change |
Last edited by: ThaKibosh at: 3/11/2016 11:38:19 AMLast edited by: ThaKibosh at: 3/11/2016 11:38:55 AMLast edited by: ThaKibosh at: 3/11/2016 11:39:09 AMLast edited by: ThaKibosh at: 3/11/2016 11:40:28 AM |
|
| 3/11/2016 11:52 AM | |
|
Joined: 6/3/2014 Last visit: 12/12/2025 Posts: 660 Rating:
|
Hello ThaKibosh, I guess if you call an .exe file written in C you could also use this code:
"The following instructions show how to use a C script to bring a selected window into the foreground. In the first example code you just have to change the MS Access handle with the Windows Explorer handle:
|
Last edited by: H.J. at: 3/11/2016 11:54:02 AM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
| 3/14/2016 8:09 AM | |
|
Joined: 5/31/2011 Last visit: 8/7/2025 Posts: 190 Rating:
|
Thx HJ But in WinCC Advanced there is only VBS available. |
Follow us on