5/23/2016 11:22 PM | |
Joined: 3/30/2011 Last visit: 7/19/2025 Posts: 739 Rating:
|
Hello, 1xp8012-10 is HTL encoder 1xp8012-20 is TTL encoder. please see links in this post. Where this encoder is connected?? |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
This contribution was helpful to
1 thankful Users |
5/24/2016 1:19 AM | |
Posts: 3 Rating:
|
thank you very much but I don't sure, so I can't changer please you check again I have attached drawings to you, plese help me Can I buy encoder 1XP8012-10/1024 to replace for encoder 1XP8012-20/1024 ? Attachment1525-03A-01.zip (582 Downloads) |
Last edited by: ngoclan at: 5/24/2016 1:21:05 AMLast edited by: Min_Moderator at: 5/24/2016 11:56:16 AMAttached pdf |
|
5/24/2016 12:54 PM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello After going through your drawing, I am assuming that the Encoder is connected to the SMC30 Encoder Module : SENSORMOD SMC30 6SL3055-0AA00-5CA1 The Technical description of SMC30 : SINAMICS SENSOR MODULE SMC30 INCREMENTAL ENCODER: TTL/HTL OR KOMBI ENCODER SSI WITH INCREMENTAL TRACES WITHOUT DRIVE-CLIQ CABLE So theoretically you should be able to use HTL as well as TTL encoders . However pl check the connection details in the attached description for HTL and TTL encoders. Also Pl change the Encoder type in the System configuration and download before connecting a TTL encoder in place of an HTL encoder , otherwise the 5V TTL encoder may ne damaged by 24V supply. Hope this helps Cheers Navnag AttachmentSMC30.pdf (459 Downloads) |
Last edited by: Navnag at: 5/24/2016 7:49:27 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to
2 thankful Users |
5/24/2016 1:42 PM | |
Joined: 9/27/2006 Last visit: 9/11/2025 Posts: 12406 Rating:
|
Hello ngoclan; HTL and TTL electronic circuitry have different voltage levels and 0-1 transition levels, so they cannot be used as simple one-to-one replacement to one another. Of course, this being electronic circuitry there are circuit modifications that can be added so that their output voltage levels are matched. But this requires a good understanding of electronics and of each particular circuit. For details on HTL/TTL circuits and adaptation circuitry between them , you could have a look at this webpage, for example. https://www.posital.com/en/products/communication-interface/incremental/incremental-encoders.php There are many more such posts on the web, if you want other points of view. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on