(3)| 6/3/2016 7:29 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hio AGrS, I was thinking about your problem. There were only two possibilities: s7_sampletime not used so incorrect incrementing of the timer or something with the cycle time of the AS-> When it goes to protected mode, the interrupt OB cycle times are halved in order to improve the cycle time. If still not OK, the CPU will slow down the OB's even more.... But this you would have noticed. Can you tell me which blocks you used exactly? I want to test out your problem, because that's is real "shitty" if something happens like that....
|
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 6/7/2016 9:54 AM | |
|
Posts: 112 Rating:
|
Hi Oreca, I had the following time blocks in my system, but I did not trigger them. |
Follow us on