(2)| 4/2/2008 4:31 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello JSMTek; The PA coupler is transparent to the DP configurator; there is no gsd file for the coupler. It holds no DP or PA address and when using a IM-152, it is used to power the PA slaves and collect the data on the PA side for the DP exchange through the link. The gsd file you insert in the configurator must be built sepecially for the DP/PA link, using Siemens' GSDtool program. It requires a Java virtual machine on your computer (free download)and the individual gsd files for all PA slaves you intend to setup on the link. Here is a link to the GSDtool download and help Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/2/2008 4:32 PM |
|
This contribution was helpful to
|
|
| 4/2/2008 4:57 PM | |
|
Joined: 1/4/2008 Last visit: 12/22/2025 Posts: 703 Rating:
|
Hello, did you see this FAQ? http://support.automation.siemens.com/WW/view/en/22729270 |
Follow us on