(0)| 7/8/2016 12:07 PM | |
|
Joined: 12/10/2015 Last visit: 12/22/2025 Posts: 11 Rating:
|
Hi. I have a VB script on a TP1200 Confort panel, where I communicate with a webserver.
Works fine. Then I want to read the answer from the webserver (It can be OK, ERROR, NO JOB etc.). I use this code. It works fine on my pc with runtime, but the panel not create a stream-object.
Is there another way I can read the answer from the server without using ADODB.Stream? It seems like it is not supported ind Windows CE (the operating system of the panel) I have to get the answer in a tag, så I can take some actions. Bedst regards |
Follow us on