(0)| 4/10/2008 8:15 AM | |
|
Joined: 4/6/2006 Last visit: 11/21/2025 Posts: 604 Rating:
|
Hi Tiago_Rosa, It looks like the settings are correct as far as we can see. Then I'm almost sure the Media Converters are the worst concerns. Why do't you have a look at the Scalance X101-1 mediaconverters? These are tested in combination with the HSR. If you use different Mediaconverters it could occur that they are not fully protocol tranpsarant which could cause severe problems in the ring or they are not fast enough. For more information about the available Media Converteers Scalance X101-1 I think it's the best to have a look in the manual. Manual Scalance X101-1 |
Last edited by: INS at: 4/10/2008 8:22 AMBest regards, |
|
Follow us on