(1)| 7/18/2016 8:54 AM | |
|
Posts: 8 Rating:
|
Hi Christoph, I have not conneted via s7 online. I have used access point as device (Starter Scout). Please see the screen shot |
| 7/19/2016 5:34 AM | |
|
Posts: 8 Rating:
|
Hi Christoph, I have attached a video of whats happening when I start STARTER Program. As you can see the program can detect the Port, but with a question mark. And I cant accept it in my project as the accept button is greyed out. By the way for your info I can connect to other G120 drives without any issues using USB.S7USB.1 as PG/PC interface and directlt connecting the USB cable to drives. AttachmentVideo_2016-07-19_112240.wmv (1341 Downloads) |
| 7/19/2016 10:11 AM | |
|
Posts: 8 Rating:
|
Hi Christoph, Please find my attached file. It gives the drive details and all the installed devices. As can be seen its a G150 Drive and all the devices G130, G150 & S120 with CU320-2DP are installed Regards Nandan AttachmentDrive Details & Installed devices.pdf (1363 Downloads) |
| 7/19/2016 10:29 AM | |
|
Joined: 5/12/2006 Last visit: 1/22/2026 Posts: 22807 Rating:
|
Hello, no the SSP is not installed. From the Typeplate you have a SInamics G150 and from the Video it shows the Version V4.5.0.2. And now in your list for the Type G150 you have installed only Version V4.7 which matching this Type but not this Version! Please download the SSSP S120 Version 4.5 from here: https://support.industry.siemens.com/cs/ww/en/view/26233208 You must Download the Vol1 and Vol2 from starter and extract it to the same directory then start the install and select the SSP for Version V4.5. Attention! Regards Christoph |
Last edited by: ChristophD at: 7/19/2016 10:34:32 AM |
|
This contribution was helpful to
|
|
| 7/20/2016 7:23 AM | |
|
Posts: 8 Rating:
|
Hi Christoph, Thanks a lot. downloading * installing Sinamics 4.5 worked. And I acn now connect and read VFD parameters. Thanks once again |
Follow us on