8/8/2016 9:34 AM | |
Joined: 10/11/2006 Last visit: 9/5/2025 Posts: 6038 Rating:
|
Hello, if you want to use a motor command, for example Off3, in hand mode of the IOP or control priority of the Starter, you have to connect the used digital input to Parameter p849, because the signal for p848 is given by the master control system, in this case the IOP or Starter. You can find this relation in the attached function diagram 2501. AttachmentE-2.pdf (120 Downloads) |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on